PN7462 flash programming,power reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7462 flash programming,power reset

ソリューションへジャンプ
5,184件の閲覧回数
sanath_rai
Contributor III

Hello,

I am working on pn7462 development kit, nfc based application.

I have downloaded pn7462 firmware from the nxp site and have dumped the example codes.

I am using lpclink to debug the board.but I am not able to flash the code into pn7462 ,that is after power on reset I need to dump the code again to run the application.how to make it run from the flash so that even after power reset application should start running .

Thank you

Sanath Rai

タグ(1)
0 件の賞賛
返信
1 解決策
4,942件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hello,

Did you program the board with examples in Debug version? If yes, please use Release version instead.

Have a great day,
Kan

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

5 返答(返信)
4,943件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hello,

Did you program the board with examples in Debug version? If yes, please use Release version instead.

Have a great day,
Kan

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

4,804件の閲覧回数
thiago_machado
Contributor III

After a power reset, the firmware wasn't lauching. When compile it in Release mode, it's working fine now. Thanks!

0 件の賞賛
返信
4,942件の閲覧回数
sanath_rai
Contributor III

Hi Kan_Li,

Yes ,it was building on debug version.

Programmed on Release version now its flashed.

Thank you,

Regards,

Sanath Rai

0 件の賞賛
返信
4,942件の閲覧回数
sachin_singh
Contributor II

Hi Sanath Rai & Kan_Li,

Thanks for this post, I faced the same problem.

After going through post I resolved it(debug to release).

Regards

0 件の賞賛
返信
4,354件の閲覧回数
amighri
Contributor II

Hi @sachin_singh ,

How did it work for you ? is it enough to build the release version or did you debug it ?

Thanks in advace. 

 

0 件の賞賛
返信