PN7462 Stack Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7462 Stack Issue

1,691 Views
mukadder
Contributor III

Why local variables in a SPIM R/W function ( access to / from a NOR flash ) fails read / write to SPIM bus.

However, Accessing to/from NOR flash using global variables with the same SPIM R/W function results with no error.

What can be the problem? By the way, the project uses no RTOS.

Regards.

0 Kudos
Reply
1 Reply

1,640 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Looks like a software issue, is the optimization too high? Please try a lower level and check if it works.

Hope that helps,

Have a great day,
Kan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply