PN7462 Rf Callback

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PN7462 Rf Callback

2,093 次查看
sachindia86
Contributor I

Hi NXP,

In PN7462 dev kit, DoorAccess Demo Example, we get a Rf Callback whenever a card is detected. Is it possible to get a callback whenever a card is removed from the reader?

Thanks

标签 (2)
标记 (1)
0 项奖励
回复
2 回复数

2,045 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

Once the card has been detected, there is not something like to check via RF. It is rather necessary to send some commands to verify if the Tag is still on the field. In the following thread there is the SW recommendation for this: https://community.nxp.com/message/1304209?commentID=1304209#comment-1304209 

Hope it helps!

BR,

Ivan.

0 项奖励
回复

2,045 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

Once the card has been detected, there is not something like to check via RF. It is rather necessary to send some commands to verify if the Tag is still on the field. In the following thread there is the SW recommendation for this: https://community.nxp.com/message/1304209?commentID=1304209#comment-1304209 

Hope it helps!

BR,

Ivan.

0 项奖励
回复