PN7462 Rf Callback

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7462 Rf Callback

2,063 Views
sachindia86
Contributor I

Hi NXP,

In PN7462 dev kit, DoorAccess Demo Example, we get a Rf Callback whenever a card is detected. Is it possible to get a callback whenever a card is removed from the reader?

Thanks

Labels (2)
Tags (1)
0 Kudos
Reply
2 Replies

2,015 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Once the card has been detected, there is not something like to check via RF. It is rather necessary to send some commands to verify if the Tag is still on the field. In the following thread there is the SW recommendation for this: https://community.nxp.com/message/1304209?commentID=1304209#comment-1304209 

Hope it helps!

BR,

Ivan.

0 Kudos
Reply

2,015 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Once the card has been detected, there is not something like to check via RF. It is rather necessary to send some commands to verify if the Tag is still on the field. In the following thread there is the SW recommendation for this: https://community.nxp.com/message/1304209?commentID=1304209#comment-1304209 

Hope it helps!

BR,

Ivan.

0 Kudos
Reply