PN7462 RX optimization for ISO14443A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7462 RX optimization for ISO14443A

1,638 Views
bds1
Contributor I

I'm trying to optimize the PN7462 RX parameters (RxHpcf, RxGain and MinLevel) for ISO14443A card detection and communication. I have a few questions about this:

- Is there a documented procedure to do this?

- Which RxHpcf, RxGain and MinLevel EEPROM parameters are used during technology detection, collision resolution and activation?

- Which RxHpcf, RxGain and MinLevel EEPROM parameters are used during ISO14443A communication at 106 kbps?

0 Kudos
Reply
1 Reply

1,538 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

You can read the values stored in EEPROM by making use of the cockpit tool. So that you can take them as reference: 

NFC Cockpit|NXP 

I hope this helps.

Reagards,

Ivan.

0 Kudos
Reply