PN7462 NFC reader collision errors in NFC Cockpit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7462 NFC reader collision errors in NFC Cockpit

1,930件の閲覧回数
jasonee
Contributor I

I'm working with a PN7462 NFC reader and am seeing a collision error every time I attempt to read from a ISO 14443-A RFID card. Hardware wise, The VNA shows that the filter is turned fairly close to the 13.56MHz, and the output power looks good. I can even see that the card is responding to a REQA command, yet the PN7462 is unable to understand the data. I was able to successfully read the result from the REQA command once, but this was out of 100's of attempts.

I cannot find any documentation that points me towards what causes the collision errors beyond attempts to read more than one card at once (which I'm not trying). I suspect it has something to do with the antenna tuning. I'm a novice when it comes to wireless communication in general, so I really do not have any good reason to believe the tuning is the issue outside of the fact that the communication isn't working. On the other hand, the VNA results look to be in line with what is expected according to the AN11532 application note. 

Any suggestions on experiments would be helpful. Thanks for reading

タグ(1)
0 件の賞賛
返信
1 返信

1,788件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

There is an app note for PN7462 antenna design, please refer to https://www.nxp.com/docs/en/application-note/AN11706.pdf  for details.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信