PN7462 Example ex_phExMain in RTOS configuration is not running on development board OM27462CDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7462 Example ex_phExMain in RTOS configuration is not running on development board OM27462CDK

1,957件の閲覧回数
haransai
Contributor I

Dear Ladies and Gentlemen,

 

I use following system:

-LPCXpresso V8.2.2 [Build 650]

-Eclipse plugin: com.nxp.pn7xxxxx.update-8.0.0-SNAPSHOT-163.zip

-Development board OM27462CDK

I installed and followed the instruction in UM10883.pdf.

 

According to manual of UM10883 the example PN7462AU_ex_phExMain should run with RTOS. Compilation runs fine also debugging. 

 

I randomly get the message "stalled on bus operation" in the status bar of LPCXpresso and the led's  on the board are not glowing and the board is not giving any response to the code(it is not reading any card). 

 

Can anyone help me?

What am I doing wrong?

 

 

Thank you very much and best regards

haran sai

0 件の賞賛
返信
2 返答(返信)

1,543件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

I just ran the project and it is working fine, the leds stop shifting when PNEV7462B detects a tag, once the tag is not within the field they shift again. 

Make sure the power of PNEV7462B is stable and the project runs normally (it is not stucked in any function or interrupt).

Screen captures:

pastedImage_3.png

pastedImage_4.png

pastedImage_5.png

Regards,

Ivan.

0 件の賞賛
返信

1,543件の閲覧回数
haransai
Contributor I

Dear Sir,

 

I am using following system:

-LPCXpresso V8.2.2 [Build 650]

-Eclipse plugin: com.nxp.pn7xxxxx.update-8.0.0-SNAPSHOT-163.zip

-Development board OM27462CDK

I installed and followed the instruction in UM10883.pdf.

 

According to manual of UM10883 the example PN7462AU_ex_phExMain is running properly.

 

And I randomly get the message "stalled on bus operation" in the status bar of LPCXpresso.

what is meant meant by stalled on bus operation and why it is coming frequently and I am also facing another error  

16: Target error from status-poll: Ee(FF). Redlink interface error 255.

 

Can u pls help me sir ?

What am I doing wrong?

 

 

Thank you very much and best regards

haran sai

0 件の賞賛
返信