PN7462 Development Kit Firmware Program Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7462 Development Kit Firmware Program Problem

3,987 Views
hirensorathiya
Contributor I

Hello NXP Team,

Recently we are working on PN7462 Development kit and tested using NXP Cockpit Application. But after installed MCUXpresso IDE and download SDK for PN7462. it builts successful but when I try to debug it, IDE fire one error which in mention below, kindly find it below and guide me on same. 

########################################ERROR#################################################

Error in final launch sequence
Failed to execute MI command:
-target-select extended-remote | crt_emu_cm_redlink -msg-port=50453 -g -mi -2 -pPN7462AU-C3-00 -vendor=NXP -ConnectScript=PN7xxxxx_Connect.scp -ResetScript=PN7xxxxx_Reset.scp -reset= -ProbeHandle=1 -CoreIndex=0 --flash-driver PN7xxxxx_158k.cfx --telnet 3330
Error message from debugger back end:
error starting child process 'crt_emu_cm_redlink -msg-port=50453 -g -mi -2 -pPN7462AU-C3-00 -vendor=NXP -ConnectScript=PN7xxxxx_Connect.scp -ResetScript=PN7xxxxx_Reset.scp -reset= -ProbeHandle=1 -CoreIndex=0 --flash-driver PN7xxxxx_158k.cfx --telnet 3330': CreateProcess: No such file or directory
error starting child process 'crt_emu_cm_redlink -msg-port=50453 -g -mi -2 -pPN7462AU-C3-00 -vendor=NXP -ConnectScript=PN7xxxxx_Connect.scp -ResetScript=PN7xxxxx_Reset.scp -reset= -ProbeHandle=1 -CoreIndex=0 --flash-driver PN7xxxxx_158k.cfx --telnet 3330': CreateProcess: No such file or directory

############################################################################################### 

Looking forward to hearing from you. Thanks in Advance

Regards

Hiren Sorathiya 

3 Replies

3,330 Views
gytiskazlauskas
Contributor II

Are you using PN7462AU FW & SW Examples Full Version - v05_07_01 ?

And if so, did you check 6.5 Building projects and 6.6 Running and debugging the example projects from UM10883 PN7462AU Quick Start Guide - Development Kit and follow the steps?

3,329 Views
hirensorathiya
Contributor I

Thanks for your reply. 

Program Problem is solved , it is working good.

0 Kudos
Reply

3,329 Views
gytiskazlauskas
Contributor II

So if you can, than mark that this question is answered.

0 Kudos
Reply