PN7462 Development Kit Firmware Program Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PN7462 Development Kit Firmware Program Problem

3,863 次查看
hirensorathiya
Contributor I

Hello NXP Team,

Recently we are working on PN7462 Development kit and tested using NXP Cockpit Application. But after installed MCUXpresso IDE and download SDK for PN7462. it builts successful but when I try to debug it, IDE fire one error which in mention below, kindly find it below and guide me on same. 

########################################ERROR#################################################

Error in final launch sequence
Failed to execute MI command:
-target-select extended-remote | crt_emu_cm_redlink -msg-port=50453 -g -mi -2 -pPN7462AU-C3-00 -vendor=NXP -ConnectScript=PN7xxxxx_Connect.scp -ResetScript=PN7xxxxx_Reset.scp -reset= -ProbeHandle=1 -CoreIndex=0 --flash-driver PN7xxxxx_158k.cfx --telnet 3330
Error message from debugger back end:
error starting child process 'crt_emu_cm_redlink -msg-port=50453 -g -mi -2 -pPN7462AU-C3-00 -vendor=NXP -ConnectScript=PN7xxxxx_Connect.scp -ResetScript=PN7xxxxx_Reset.scp -reset= -ProbeHandle=1 -CoreIndex=0 --flash-driver PN7xxxxx_158k.cfx --telnet 3330': CreateProcess: No such file or directory
error starting child process 'crt_emu_cm_redlink -msg-port=50453 -g -mi -2 -pPN7462AU-C3-00 -vendor=NXP -ConnectScript=PN7xxxxx_Connect.scp -ResetScript=PN7xxxxx_Reset.scp -reset= -ProbeHandle=1 -CoreIndex=0 --flash-driver PN7xxxxx_158k.cfx --telnet 3330': CreateProcess: No such file or directory

############################################################################################### 

Looking forward to hearing from you. Thanks in Advance

Regards

Hiren Sorathiya 

3 回复数

3,206 次查看
gytiskazlauskas
Contributor II

Are you using PN7462AU FW & SW Examples Full Version - v05_07_01 ?

And if so, did you check 6.5 Building projects and 6.6 Running and debugging the example projects from UM10883 PN7462AU Quick Start Guide - Development Kit and follow the steps?

3,205 次查看
hirensorathiya
Contributor I

Thanks for your reply. 

Program Problem is solved , it is working good.

0 项奖励
回复

3,205 次查看
gytiskazlauskas
Contributor II

So if you can, than mark that this question is answered.

0 项奖励
回复