PN7462 Development Kit Firmware Program Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7462 Development Kit Firmware Program Problem

3,837件の閲覧回数
hirensorathiya
Contributor I

Hello NXP Team,

Recently we are working on PN7462 Development kit and tested using NXP Cockpit Application. But after installed MCUXpresso IDE and download SDK for PN7462. it builts successful but when I try to debug it, IDE fire one error which in mention below, kindly find it below and guide me on same. 

########################################ERROR#################################################

Error in final launch sequence
Failed to execute MI command:
-target-select extended-remote | crt_emu_cm_redlink -msg-port=50453 -g -mi -2 -pPN7462AU-C3-00 -vendor=NXP -ConnectScript=PN7xxxxx_Connect.scp -ResetScript=PN7xxxxx_Reset.scp -reset= -ProbeHandle=1 -CoreIndex=0 --flash-driver PN7xxxxx_158k.cfx --telnet 3330
Error message from debugger back end:
error starting child process 'crt_emu_cm_redlink -msg-port=50453 -g -mi -2 -pPN7462AU-C3-00 -vendor=NXP -ConnectScript=PN7xxxxx_Connect.scp -ResetScript=PN7xxxxx_Reset.scp -reset= -ProbeHandle=1 -CoreIndex=0 --flash-driver PN7xxxxx_158k.cfx --telnet 3330': CreateProcess: No such file or directory
error starting child process 'crt_emu_cm_redlink -msg-port=50453 -g -mi -2 -pPN7462AU-C3-00 -vendor=NXP -ConnectScript=PN7xxxxx_Connect.scp -ResetScript=PN7xxxxx_Reset.scp -reset= -ProbeHandle=1 -CoreIndex=0 --flash-driver PN7xxxxx_158k.cfx --telnet 3330': CreateProcess: No such file or directory

############################################################################################### 

Looking forward to hearing from you. Thanks in Advance

Regards

Hiren Sorathiya 

3 返答(返信)

3,180件の閲覧回数
gytiskazlauskas
Contributor II

Are you using PN7462AU FW & SW Examples Full Version - v05_07_01 ?

And if so, did you check 6.5 Building projects and 6.6 Running and debugging the example projects from UM10883 PN7462AU Quick Start Guide - Development Kit and follow the steps?

3,179件の閲覧回数
hirensorathiya
Contributor I

Thanks for your reply. 

Program Problem is solved , it is working good.

0 件の賞賛
返信

3,179件の閲覧回数
gytiskazlauskas
Contributor II

So if you can, than mark that this question is answered.

0 件の賞賛
返信