PN7220 Reference Hardware Design & PNEV7220BP1 Design Files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7220 Reference Hardware Design & PNEV7220BP1 Design Files

Jump to solution
2,418 Views
mcihangir
Contributor II

Hi NXP  Team and @ KellyLi,

 

I need reference hardware design for PN7220  and design files of PNEV7220BP1 EVB.

Can you please provide me a reference schematic design in PDF for PN7220 and a layout design for PNEV7220BP1?

 

Thanks!

Tags (1)
0 Kudos
Reply
1 Solution
2,337 Views
Tomas_Parizek
NXP Employee
NXP Employee
Hello mcihangir,

The PN7220 and PN7221 are fully pin-to-pin compatible. From the HW point of view, it is the same IC. The different between PN7220 and PN7221 is that the PN7221 supports "Apple Enhanced Contactless Polling" feature.

BR
Tomas

View solution in original post

4 Replies
2,398 Views
Tomas_Parizek
NXP Employee
NXP Employee

Hello mcihangir, 

 

See the required data in the attachment ! 

BR

Tomas 

2,387 Views
mcihangir
Contributor II

Hi @Tomas_Parizek 

Well received. 

Thanks for the prompt reply. 

One more small question, are PN7220 and PN7221 fully pin-to-pin compatible? I couldn't find the Hardware Design Guide document for the PN7220 IC from the link below, is there no such document?

https://www.nxp.com/products/PN7220

BR
Mehmet

 

0 Kudos
Reply
2,338 Views
Tomas_Parizek
NXP Employee
NXP Employee
Hello mcihangir,

The PN7220 and PN7221 are fully pin-to-pin compatible. From the HW point of view, it is the same IC. The different between PN7220 and PN7221 is that the PN7221 supports "Apple Enhanced Contactless Polling" feature.

BR
Tomas
2,323 Views
mcihangir
Contributor II
Hello @Tomas_Parizek,

Thanks for your great support.

0 Kudos
Reply