PN7160B - CPOL Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7160B - CPOL Configuration

ソリューションへジャンプ
2,476件の閲覧回数
michael_d_1983
Contributor I

Hello,

As described in PN7160 Datasheet, 11.2.2.2 SPI-bus configuration options:

In order to select SPI-bus interface for host communication, some EEPROM settings are
programmed during production.
Four versions can be configured depending on CPOL/CPHA EEPROM setting.
The selection between interfaces is fused during IC manufacturing so that different
ordering numbers for the SPI-bus version.

I have not found any information on different ordernumbers that affect the settings.
Is this an error?

Thanks,

Michael

0 件の賞賛
返信
1 解決策
2,405件の閲覧回数
Fabian_R
NXP TechSupport
NXP TechSupport

Hello sir,

Unfortunately, the datasheet needs an update. The PN7160 is configured as follows:

CPHA=0

IFSEL1=0

I hope this information may have been useful.

Best Regards,
Fabian

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,406件の閲覧回数
Fabian_R
NXP TechSupport
NXP TechSupport

Hello sir,

Unfortunately, the datasheet needs an update. The PN7160 is configured as follows:

CPHA=0

IFSEL1=0

I hope this information may have been useful.

Best Regards,
Fabian
0 件の賞賛
返信
2,415件の閲覧回数
Erklei
Contributor I

I think only I2C vs SPI is programmed during manufacturing. Part number ending with "A" is I2C and "B" is SPI. Clock polarity can be changed later

0 件の賞賛
返信