PN7160 stucks in doInitialize()

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7160 stucks in doInitialize()

2,938件の閲覧回数
michael_d_1983
Contributor I

Hello,

unfortunately I have a problem with the PN7160.

Board = Linux, PN7160 - SPI @ 6.25MHz

NCI library from https://github.com/NXPNFCLinux/linux_libnfc-nci/tree/NCI2.0_PN7160

PN7160 patched to the latest version from https://github.com/NXP/nfc-NXPNFCC_FW/tree/master/InfraFW/pn7160/12_50_0E

On one board it happened that the NCI stack could no longer be started - the application got stuck in doInitialize(). Restarting the system with and without removing power did not help.
I then found out that after deleting the timestamp (this is written by the NCI stack when the configuration of the PN7160 has changed) the whole system works normally again.

I then tried again to see if the error occurred again (start nfc, stop nfc, delete timestamp, start nfc again, and so on...).

The error is reproducible! Even if it sometimes takes many attempts.

My assumption is that something went wrong when writing the PN7160 config and the NCI stack then no longer starts.

Is this problem known or is there a patch that solves this problem?

An update of the configuration could paralyze the NFC functionality of our devices with this problem.

Thank you very much!

Yours sincerely,
Michael

0 件の賞賛
返信
5 返答(返信)

2,826件の閲覧回数
salt29
Contributor II

Hi @michael_d_1983  i have the same issue with the PN7150. Did you solved it? is it possible to reach the case number: 00693420?

0 件の賞賛
返信

2,748件の閲覧回数
michael_d_1983
Contributor I

Hi salt29,
I'm sorry, but I don't use the PN7150. Does everything work again if you delete the timestamp?

0 件の賞賛
返信

2,724件の閲覧回数
salt29
Contributor II

I don't see any timestamp in my routine. Can you specify where is it?

It still does not working properly. sometimes it is blocked at doInitialize(). After few try it starts again.

0 件の賞賛
返信

2,926件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @michael_d_1983 

This is the duplicated case, I have forwarded your question to the internal team, please note the update of the case number: 00693420.

0 件の賞賛
返信

2,797件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

they have applied the on-site technical support.

0 件の賞賛
返信