PN7160 current draw in Card Emulation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PN7160 current draw in Card Emulation

789 次查看
dlormand
Contributor I

I'm contemplating using the PN7160 in a field-powered Card Emulation role using a low-power microcontroller as the host.  I'm confused with the datasheet that has two Ibat sections and none of the entries seem to clearly apply.  I understand to talk to a host, the Vdd(pad) must be present, and this would indicate Full-Power Mode (per section 11.1.1).  I am thinking that the power state (11.1.2) would be Active, and the device is operating as a Listener.  Therefore, the closest scenario might be "Idle and Target Active" state in Table 35 - 4.55mA typ.

Is there a clear "right" answer?

0 项奖励
回复
0 回复数