PN7160 can't running nfcDemoApp of linux_libnfc-nci on Ubuntu 22.04 with AltI2C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7160 can't running nfcDemoApp of linux_libnfc-nci on Ubuntu 22.04 with AltI2C

1,118 Views
chiajeng
Contributor I

Hi Sir,

I can execute NfcFactoryTestApp and discovery T1~T4 tag from linux_NfcFactoryTestApp repo on Ubuntu 22.04

But same configuration (AltI2C gpio pin) with nfcDemoApp poll mode from linux_libnfc-nci repo and NCI2.0_PN7160 branch  , always stop at NfcService Init Failed  in InitMode

 

Have have one can give me advice for this problem?

Thanks

 

0 Kudos
Reply
3 Replies

1,089 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @chiajeng 

It is recommended that you do these operations again from 5.1.2 to 5.1.5 of AN13287(as the below). Then try to call the APP (./nfcDemoApp). If it doesn't work, please provide the log to us.

 

https://www.nxp.com.cn/docs/en/application-note/AN13287.pdf

0 Kudos
Reply

1,051 Views
chiajeng
Contributor I

Hi @KaiLi 

PN7160 log as attchement.

Platform information as below

Linux ix-virtual-machine 6.5.0-45-generic #45~22.04.1-Ubuntu SMP PREEMPT_DYNAMIC Mon Jul 15 16:40:02 UTC 2 x86_64 x86_64 x86_64 GNU/Linux

nfcDemoApp can't running , but that NfcFactoryTestApp can running on same environment.

Could you please give us some advice for the problem?

 

Thansk.

 

Regards,

C.J.
0 Kudos
Reply

969 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @chiajeng 

Sorry for the late reply. From analyzing the log, we recommend you to porting NFC components again.

0 Kudos
Reply