PN7150 with ESP32-S3 - Arduino Framework

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7150 with ESP32-S3 - Arduino Framework

3,607 Views
petemanzel
Contributor I

Hello all,

I am trying to get a PN7150 to work with an ESP32-S3.

I used the library of Electronic Cats without any success. 

It seems to connect to the chip but it is not reading any tag or card.

Does anyone has got this combination working?

Thanks in advance for any help.

0 Kudos
Reply
3 Replies

1,892 Views
Chri-sy
Contributor I

I am also facing the same challenge with PN7160. I am able to initialize the PN7160 but i cannot read any tap. @Julián_AragónM   could you please prioritize support on the PN7150/60 on commonly used MCUs such as EPS32, STM32 as the previous NFC model, PN532 is being phased out.

0 Kudos
Reply

3,466 Views
Joust22
Contributor I

Hey @petemanzel did you have any luck with this? I'm having the same issue, I can successfully comm with the PN1750 but can't read any tags. Using ESP32-S3-MINI-1 and Electronic Cats library

0 Kudos
Reply

3,576 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @petemanzel,

I apologize for the inconvenience this may cause, but this seems out of our support scope, I would suggest contacting the creators of this library for additional support.

You can instead try our examples on the chip, following the documentation on PN7150's page:

Best regards,
Julián.

0 Kudos
Reply