PN7150 returning (A1) error code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7150 returning (A1) error code

1,737件の閲覧回数
tyler4
Contributor I

Hi, I am working on bringing up a PN7150 to use with DESFire EV1/EV2 cards. I am setting up a simple configuration (let me know if you need details) and running a loop every second to check the INT line and read in data if the line is set. When I continuously hold a DESFire card to the NFC, the card will be found successfully ~40% of the time and I will read a RF_INTF_ACTIVATED_NTF successfully. The other ~60% of the time when I read the PN7150 I am seeing a CORE_GENERIC_ERROR_NTF with status DISCOVERY_TARGET_ACTIVATION_FAILED (A1). My question is, does this hint at more of a HW problem that needs fixing? Or does this sound like something wrong with how the PN7150 is configured, or the DH interaction with it. Thanks 

タグ(2)
0 件の賞賛
返信
1 返信

1,486件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please accept my apologies, but currently DESfire is not supported in the current Library.

Thank you for your comprehension.

Regards,

Ivan.

0 件の賞賛
返信