PN7150 debug problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7150 debug problem

3,202件の閲覧回数
gddw1954
Contributor I

Hello!

   I ported PN7150 to MTK's Android 9.0 based on AN11690 manual. However, I encountered errors in the log during startup, and there is no response when swiping the card. Can you please help me troubleshoot this issue? Thank you!

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

3,090件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi 

 

From the log file, there is an error 

2023-09-15 10:54:01.902 3404-3539/? D/NxpNciR: len = 5 > 4002020500
2023-09-15 10:54:01.902 3404-3539/? D/NxpTml: PN54X - Posting read message.....
2023-09-15 10:54:01.902 3404-3542/? D/NxpHal: read successful status = 0x0
2023-09-15 10:54:01.903 3404-3542/? D/NxpHal: phNxpNciHal_print_res_status: response status =STATUS_SYNTAX_ERROR

 

In case the NCI package is malformed (wrong length for example), STATUS_SYNTAX_ERROR is returned.

 

Regards

Daniel

 

 

0 件の賞賛
返信