PN7150 cannot configure NXPNCI settings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7150 cannot configure NXPNCI settings

1,038件の閲覧回数
jimmytseng
Contributor I

Hello :

We use the PN7150 with KL17M6V MCU. Frequent PN7150 can not configure NXPNCI settings.

Original can communicate with the PN7150 normally, but after a while can not communicate with the PN7150, The following is an error message.I measured the I2C signal is perfect

++++++++++++++++ GID7150 start +++++++++++++++++
[00]NbBytes:4
NbBytes:6
Get tag cmd size: 9
Get tag cmd data: 0x40 0x03 0x06 0x00 0x01 0xA0
0x03 0x01 0x08
Error: cannot configure NXPNCI settings

How do I deal with this kind of problem?

0 件の賞賛
返信
0 返答(返信)