Mifare Classic 1K Authentication error 201 while porting Nxp-NFC-Reader Library over Keil uVision4.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mifare Classic 1K Authentication error 201 while porting Nxp-NFC-Reader Library over Keil uVision4.

2,939件の閲覧回数
sameerhuddar
Contributor I

Hello!

I am working on simple smart card Mifare Classic 1K application downloaded from NXP website to detect contact less cards and further perform read/write operation. I am using CLEV663B blueboard v3.0.

I've ported the application that is running on LPC1769 controller interfaced with CLRC663 reader IC through I2C protocol over Keil uVision4 IDE.The program is being compiled and detecting cards but during authentication process I am facing an issue and getting an error 0x201 ((PH_ERR_IO_TIMEOUT) and authentication failed during execution of 'phalMfc_Authenticate' function. After tying to debug through the whole functions being called, i found that the error is generated in either "phhalHw_Rc663_Cmd.c" or "phhalHw_Rc663_Int.c" file.

I am using UART0 for displaying the information.

Kindly guide with any possible solutions or reasons for the error. Please see the attached image for reference

0 件の賞賛
返信
0 返答(返信)