PN7150 Type 4 card emulation with RPi/Python

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7150 Type 4 card emulation with RPi/Python

4,639件の閲覧回数
david_nash
Contributor I

Hello NXP community,

I am at a beginner level in both programming hardware and NFC, so please excuse any incorrect terminology I use. I have a PN7150 on a OM5578 kit on a Raspberry Pi 4. My ultimate goal is to write Python script that will write text onto the NFC card and do Type 4 Card emulation so that I can transfer that text to an NFC reader device.

It looks like the nfcDemoApp does not support Type 4 Card emulation, so I am wondering if there are any resources I can be directed to that will allow me to test out Type 4 Card emulation capabilities of the PN7150/OM5578 on the Raspberry Pi. 

From my search online, there does not seem to be any Raspberry Pi/Python Type 4 Card emulation support for the PN7150. Although I can find some C and C++ resources for the PN532 or PN7120, I read that those resources do not support PN7150 and those models interface on the SPI bus instead of the I2C bus. 

If I could get some help interfacing the PN7150 via I2C bus on the Raspberry Pi 4 (using Python) to write data onto the PN7150 and emulate a Type 4 card (ISO/IEC 14443 A and/or B), that would be VERY helpful. 

Thank you in advance.

#nfc pn7510 pn7150‌ #pn7150rpi#card emulation#iso1443 4/3 type a and b#i2c protocol#raspberrypi#nfc om5578‌ #nfc

0 件の賞賛
返信
1 返信

4,584件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信