PN7150 NFC Controller Initialization Failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PN7150 NFC Controller Initialization Failed

2,914 次查看
wjzhang99
Contributor I

I am trying to build  nfcDemoApp application to run on imx6 based target using PN7150 NFC Controller. I have followed NXP AN11697 document to build kernel driver and "nfcDemoApp" application as well as install the library. When I run the demo application on the target, it says "NfcService Init Failed Leaving...".

By checking the source code, I know it is due to API function call nativeNfcManager_doInitialize() returning non-zero value. But there is no further detailed explanation of the cause in the "Linux_NFC_API_Guide.html" file.

Can anybody tell me what might be causing non-zero return value of that API function call? How do I know whether the kernel driver or the library were correctly built and installed?

Thank you.

William

0 项奖励
回复
1 回复

2,380 次查看
jimmychan
NXP TechSupport
NXP TechSupport
0 项奖励
回复