PN7150 NCI Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7150 NCI Problem

16,834件の閲覧回数
hanpengfei_666
Contributor II

i checked the pn7150 user guid and found that the NCI is not comprehensive,i would like to know whether there is a detailed explanation of NCI?

タグ(1)
9 返答(返信)

16,572件の閲覧回数
hanpengfei_666
Contributor II

from the NFC Forum,i don't find the NCI document ,can you help me find the document ? thank you!

0 件の賞賛
返信

16,572件の閲覧回数
Strooom
Contributor II

Hi, unfortunately, the NFC Forum specifications are only free of charge for members. If you are not a member, you need to purchase them and they are expensive.

Some years ago they were still free of charge on their website, so many older website/articles still refer to them as such but they are no longer available.

Here is my github repository for a PN7150 driver. Could be usefull to answer some questions on NCI you have.

https://github.com/Strooom/PN7150

Engineer by Day, Maker by Night
0 件の賞賛
返信

16,572件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please contact the NFC Forum for more details about their process to get it.

BR,

Ivan.

0 件の賞賛
返信

16,566件の閲覧回数
hanpengfei_666
Contributor II

Enable Low Power Card Detection Mode ,i learn from https://www.nxp.com.cn/docs/en/application-note/AN11757.pdf

There is my code , uint8_t NxpNci_CORE_CONF_EXTN[]={ 0x20, 0x02, 0x0D, 0x03, /* CORE_SET_CONFIG_CMD */

0xA0, 0x40, 0x01, 0x00, /* TAG_DETECTOR_CFG */

0xA0, 0x41, 0xFF, 0x04, /* TAG_DETECTOR_THRESHOLD_CFG */

0xA0, 0x43, 0x00, 0x50 /* TAG_DETECTOR_FALLBACK_CNT_CFG */

};

Oscilloscope screenshot as follow, i know that it is regular mode , i guess it may be my configuration problem. To verify my problem, I want to know the answer when i send NxpNci_CORE_CONF_EXTN[].

Thank you for your guidance.

On 9/17/2019 23:36,IvanRuiz<[email protected]> wrote:

|

|

NXP Community

|

|

Re: PN7150 NCI Problem

reply from IvanRuiz in NFC - View the full discussion

Hello,

Please contact the NFC Forum for more details about their process to get it.

BR,

Ivan.

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in NFC by email or at NXP Community

Following Re: PN7150 NCI Problem in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

|

|

0 件の賞賛
返信

16,566件の閲覧回数
hanpengfei_666
Contributor II

The problem has been solved. Thank you.IvanRuiz

15,883件の閲覧回数
su_can
Contributor I
请问您的问题是怎么解决的
0 件の賞賛
返信

16,566件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

You are welcome!

BR,

Ivan.

0 件の賞賛
返信

16,566件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please refer to the following document: https://www.nxp.com/docs/en/user-guide/UM10936.pdf 

This User Manual describes the software interfaces. For more information, you may refer to the NFC Forum NCI document.

BR,

Ivan.

16,566件の閲覧回数
hanpengfei_666
Contributor II

hollo:

from the NFC Forum,i don't find the NCI document ,can you help me find the document ? thank you!

On 9/12/2019 01:56,IvanRuiz<[email protected]> wrote:

|

|

NXP Community

|

|

Re: PN7150 NCI Problem

reply from IvanRuiz in NFC - View the full discussion

Hello,

Please refer to the following document: https://www.nxp.com/docs/en/user-guide/UM10936.pdf

This User Manual describes the software interfaces. For more information, you may refer to the NFC Forum NCI document.

BR,

Ivan.

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in NFC by email or at NXP Community

Following Re: PN7150 NCI Problem in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

|

|

0 件の賞賛
返信