PN7150 LPCUSBSIO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7150 LPCUSBSIO

1,538件の閲覧回数
matthew5025
Contributor I

When using the linux_libnfc-nci with LPCUSBSIO as described here, there seems to be an issue with Card Emulation. Sending a large response to the reader (~200 bytes) seems to cause the library to lock up and no longer process any other commands. 

This does not occur when using the library in alt mode, nor when using the code provided in SW4335, so it seems to be specific to the linux_libnfc-nci with LPCUSBSIO combination.

I've attached some logs in a GitHub issue (https://github.com/NXPNFCLinux/linux_libnfc-nci/issues/133)

Is this a known limitation, or is there a workaround for this issue?

Thanks!

タグ(1)
0 件の賞賛
返信
1 返信

1,509件の閲覧回数
matthew5025
Contributor I

Any help with this?

0 件の賞賛
返信