PN7150 - HardFault_Handler problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7150 - HardFault_Handler problem

2,168 Views
adrianpakosinsk
Contributor II

Hello,

I try to run example for the PN7150 chip. Unfortunately, the program stops in the function HardFault_Handler. I didn't make changes in the example project. I used the instructions from application note: AN11658.

Hardware:

OM5578/PN7150ARD

LPC1114 LPCXpresso board

Software:

LPCXpresso v8.2.2 [Build 650]

NXP-NCI LPCXpresso example (SW3241) - NXP-NCI_LPC11xx_example

What do you think could be wrong ? Maybe something should be changed in the project properties ? I checked the connections between boards and I think that are correct.

Best Regards,

Adrian Pakosinski

Labels (1)
0 Kudos
Reply
2 Replies

2,001 Views
davidwatzinger
Contributor II

Hello Adrian,

I had the same problem. I deletet some printf() functions and now the demo project works.

It´s a bit strange.

best regards

David

2,001 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Adrian,

Would you please help to check if the program still run into HardFault_Handler after you disconnect OM5578 with

LPC1114 LPCXpresso board? Thanks for your patience!


Have a great day,
Kan

0 Kudos
Reply