PN7150 - HardFault_Handler problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7150 - HardFault_Handler problem

2,128件の閲覧回数
adrianpakosinsk
Contributor II

Hello,

I try to run example for the PN7150 chip. Unfortunately, the program stops in the function HardFault_Handler. I didn't make changes in the example project. I used the instructions from application note: AN11658.

Hardware:

OM5578/PN7150ARD

LPC1114 LPCXpresso board

Software:

LPCXpresso v8.2.2 [Build 650]

NXP-NCI LPCXpresso example (SW3241) - NXP-NCI_LPC11xx_example

What do you think could be wrong ? Maybe something should be changed in the project properties ? I checked the connections between boards and I think that are correct.

Best Regards,

Adrian Pakosinski

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,961件の閲覧回数
davidwatzinger
Contributor II

Hello Adrian,

I had the same problem. I deletet some printf() functions and now the demo project works.

It´s a bit strange.

best regards

David

1,961件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Adrian,

Would you please help to check if the program still run into HardFault_Handler after you disconnect OM5578 with

LPC1114 LPCXpresso board? Thanks for your patience!


Have a great day,
Kan

0 件の賞賛
返信