PN7150 Factory TestApp

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PN7150 Factory TestApp

6,015 次查看
sivasu4098
Contributor III

Hi all,

I am using the following test application to test the MIFARE cards for nougat using PN7150 NFC chip.

nxpnfc_android_nougat/FactoryTestApp at master · NXPNFCLinux/nxpnfc_android_nougat · GitHub 

I am running the test application ./data/NfcFactoryTestApp . Getting the below response. Whenever I placed the card there is no response. how to check whether the card is reading or not . Please help me to proceed further.

----------------------------
NFC Factory Test Application
----------------------------
PN7150 NFC controller detected
Select the test to run:
     1. Continuous RF ON
     2. PRBS
Your choice: 1
Continuous RF ON test
NFC Controller is now in continuous RF ON mode - Press enter to stop

Thanks and  Regards,

Sivasubramaniyan

0 项奖励
回复
5 回复数

5,742 次查看
sivasu4098
Contributor III

In UM10936 10.1 [PN7150-NCI] extension: System configurations, CLOCK_SEL_CFG is required for configuration to activate the XTAL clock in PN7150. After this NFC tag is detected and also made changes in NfcFactoryTestApp.c  by adding the Clock configuration command.  

char NxpNci_CLK_CONF[] ={0x20, 0x02, 0x05, 0x01, 0xa0, 0x03, 0x01, 0x08};

0 项奖励
回复

5,686 次查看
skrishnan08
Contributor I

Hello Sir,

We are facing the same issue with the NFC kit. We followed your instructions by adding the 

NxpNci_CLK_CONF configurations to the NfcFactoryTestApp.c file.

Please find the sequence we followed,

1) Reset, (E9, 01)

2) NxpNci_CLK_CONF, {0x20, 0x02, 0x05, 0x01, 0xa0, 0x03, 0x01, 0x08}

3) NCICoreReset, {0x20, 0x00, 0x01, 0x00}

4) NCICoreIinit, {0x20, 0x01, 0x00}

5) Disablestandby, {0x2F, 0x00, 0x01, 0x00}

6) Rfon(). {0x2F, 0x3D, 0x02, 0x20, 0x01}

Unfortunately, we are unable to get anything while tapping the card.

0 项奖励
回复

5,742 次查看
jimmychan
NXP TechSupport
NXP TechSupport

For the details of using Factory Test Application, please refer to Chapter 5 of https://www.nxp.com/docs/en/application-note/AN11690.pdf

0 项奖励
回复

5,742 次查看
sivasu4098
Contributor III

Need more information on the below points.

1. Needed to know whether it will give the details of the detected card on sucessful read.

2. Where can i get more information about NCI commands

char NCICoreReset[] = {0x20, 0x00, 0x01, 0x01};

 char NCICoreInit[] = {0x20, 0x01, 0x00};

char NCIStartDiscovery[] = {0x21, 0x03, 0x09, 0x04, 0x00, 0x01, 0x01, 0x01, 0x02, 0x01, 0x06, 0x01};

char NCIRfOn[] = {0x2F, 0x3D, 0x02, 0x20, 0x01};

3. Is there any command sequence to test the integrity of the antenna.

0 项奖励
回复

5,742 次查看
jimmychan
NXP TechSupport
NXP TechSupport
0 项奖励
回复