PN7150 Factory TestApp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7150 Factory TestApp

6,054件の閲覧回数
sivasu4098
Contributor III

Hi all,

I am using the following test application to test the MIFARE cards for nougat using PN7150 NFC chip.

nxpnfc_android_nougat/FactoryTestApp at master · NXPNFCLinux/nxpnfc_android_nougat · GitHub 

I am running the test application ./data/NfcFactoryTestApp . Getting the below response. Whenever I placed the card there is no response. how to check whether the card is reading or not . Please help me to proceed further.

----------------------------
NFC Factory Test Application
----------------------------
PN7150 NFC controller detected
Select the test to run:
     1. Continuous RF ON
     2. PRBS
Your choice: 1
Continuous RF ON test
NFC Controller is now in continuous RF ON mode - Press enter to stop

Thanks and  Regards,

Sivasubramaniyan

0 件の賞賛
返信
5 返答(返信)

5,781件の閲覧回数
sivasu4098
Contributor III

In UM10936 10.1 [PN7150-NCI] extension: System configurations, CLOCK_SEL_CFG is required for configuration to activate the XTAL clock in PN7150. After this NFC tag is detected and also made changes in NfcFactoryTestApp.c  by adding the Clock configuration command.  

char NxpNci_CLK_CONF[] ={0x20, 0x02, 0x05, 0x01, 0xa0, 0x03, 0x01, 0x08};

0 件の賞賛
返信

5,725件の閲覧回数
skrishnan08
Contributor I

Hello Sir,

We are facing the same issue with the NFC kit. We followed your instructions by adding the 

NxpNci_CLK_CONF configurations to the NfcFactoryTestApp.c file.

Please find the sequence we followed,

1) Reset, (E9, 01)

2) NxpNci_CLK_CONF, {0x20, 0x02, 0x05, 0x01, 0xa0, 0x03, 0x01, 0x08}

3) NCICoreReset, {0x20, 0x00, 0x01, 0x00}

4) NCICoreIinit, {0x20, 0x01, 0x00}

5) Disablestandby, {0x2F, 0x00, 0x01, 0x00}

6) Rfon(). {0x2F, 0x3D, 0x02, 0x20, 0x01}

Unfortunately, we are unable to get anything while tapping the card.

0 件の賞賛
返信

5,781件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

For the details of using Factory Test Application, please refer to Chapter 5 of https://www.nxp.com/docs/en/application-note/AN11690.pdf

0 件の賞賛
返信

5,781件の閲覧回数
sivasu4098
Contributor III

Need more information on the below points.

1. Needed to know whether it will give the details of the detected card on sucessful read.

2. Where can i get more information about NCI commands

char NCICoreReset[] = {0x20, 0x00, 0x01, 0x01};

 char NCICoreInit[] = {0x20, 0x01, 0x00};

char NCIStartDiscovery[] = {0x21, 0x03, 0x09, 0x04, 0x00, 0x01, 0x01, 0x01, 0x02, 0x01, 0x06, 0x01};

char NCIRfOn[] = {0x2F, 0x3D, 0x02, 0x20, 0x01};

3. Is there any command sequence to test the integrity of the antenna.

0 件の賞賛
返信

5,781件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信