PN7120 Notifications.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7120 Notifications.

1,848件の閲覧回数
tewexor600
Contributor I

Hello, I am currently working with two PN7120 implemented in development boards ( NFC_click ). I am successfully communicating over I2C using a pic18 with the PN7120 using the NCI.

I configured the PN7120 using RF_DISCOVER_MAP_CMD and RF_DISCOVER_CMD getting the proper Responses with the Status 0x00 (ok). I should now be getting the notification RF_FIELD_INFO_NTF.

I have not recieved any notifications at any point.

As an example the initial CORE_RESET_CMD should result in a response and then a notification, there is no notificiation ever.

If anyone could assist me, or point me in the right direction, I would be grateful.

Kind regards

0 件の賞賛
返信
1 返信

1,771件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi,

Hope you are doing great, have you tried following the exact timings and commands using one of our board with the PN7120, like a FRDM K64 ?

just to confirm anything in the procedure is correct.

Have a great day !

BR

Jonathan

0 件の賞賛
返信