PN532 - connecting to Android

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN532 - connecting to Android

5,424 Views
erichnast
Contributor I

I am using the NXP PN532 NFC device in a new project. It has been possible to establish peer-to-peer communication between two bits of hardware.

 

I have however not been able to establish a link to an Android phone.

 

After initializing the hardware as a Target and issuing a TgInitAsTarget. I get a response from the Andriod phone.

When I issue the TgGetData command, the status reply from the phone is “The PN532 configured as target has been released by its

initiator “

Tags (1)
0 Kudos
Reply
1 Reply

3,100 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Erich,

I found some answers might be helpful for your issue, please kindly refer to java - The PN532 configured as target has been released by its initiator - Stack Overflow for more details.


Wish it helps.

Have a great day,
Kan Li
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply