PN532 TransportData Questions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN532 TransportData Questions

1,918件の閲覧回数
kimhyungjun
Contributor I

I know that PN532 is a transferable byte 262byte, but 64byte is sent when it is sent in P2P Initiator mode. How do I send more than 64 bytes?

 

Perhaps it is because the value of LRi in ATR_REQ is 00 and only 64byte data is checked. How can I change this value?

0 件の賞賛
返信
1 返信

1,908件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @kimhyungjun ,

 

The command of InDataExchange can be used for that purpose, and there is an example in Fig 103., please refer to https://www.nxp.com/docs/en/user-guide/141520.pdf for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信