PN532 TransportData Questions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN532 TransportData Questions

1,934 Views
kimhyungjun
Contributor I

I know that PN532 is a transferable byte 262byte, but 64byte is sent when it is sent in P2P Initiator mode. How do I send more than 64 bytes?

 

Perhaps it is because the value of LRi in ATR_REQ is 00 and only 64byte data is checked. How can I change this value?

0 Kudos
Reply
1 Reply

1,924 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @kimhyungjun ,

 

The command of InDataExchange can be used for that purpose, and there is an example in Fig 103., please refer to https://www.nxp.com/docs/en/user-guide/141520.pdf for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply