PN532 PICC emulation mode issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN532 PICC emulation mode issues

1,276 Views
euttsov
Contributor I

Hi all. I am trying to emulate PICC 14443-A card with PN532 using HSU communication mode with Microsoft IoT bindings libraries. 

Here is my InitAsTarget command:

(modeInitialized, retData) = pn532.InitAsTarget(
                                        TargetModeInitialization.PiccOnly,
                                        new TargetMifareParameters() { Atqa = new byte[] { 0x08, 0x00 }, Sak = 0x60 },
                                        new TargetFeliCaParameters() { NfcId2 = new byte[] { 0x01, 0xFE, 0xA2, 0xA3, 0xA4, 0xA5, 0xA6, 0xA7 }, Pad = new byte[] { 0xC0, 0xC1, 0xC2, 0xC3, 0xC4, 0xC5, 0xC6, 0xC7 } },
                                        new TargetPiccParameters() { NfcId3 = new byte[] { 0xAA, 0x99, 0x88, 0x77, 0x66, 0x55, 0x44, 0x33, 0x22, 0x11 }, GeneralTarget = new byte[0], HistoricalTarget = new byte[0] });

I tested two cases:
1) invoke pn532.InitAsTarget() command in cycle

2) split pn532.InitAsTarget() command into two separate commands:
2.a) one write TgInitAsTarget and read ACK
2.b) second just wait for response from pn532 when external reader appeared

In the first case the phone read a module for a very long time, but finally I got the NDEF from records from the module, providing them by host.
In the second case the phone never got info from the module. 

I decided to dump NFC exchange between phone and module by Proxmark 3 and here what I got:

This is dump for second case - TgInitAsTarget written into PN532, ack received and I waiting for TgInitAsTarget response from UART.

StartEndSrcData (! denotes parity error)CRCAnnotation
        0.0        73.2  Rdr 52(7)                                                                          WUPA
      165.5       340.1  Tag 08  00                                                                         
      886.1      1237.8  Rdr 50  00  57  cd                                                             ok  HALT
    64599.4     64672.6  Rdr 52(7)                                                                          WUPA
   502345.7    502418.9  Rdr 52(7)                                                                          WUPA
   502563.1    502577.3  Tag 01(0)                                                                          
   503231.9    503583.5  Rdr 50  00  57  cd                                                             ok  HALT
   566953.4    567026.5  Rdr 52(7)                                                                          WUPA
  1004770.5   1004843.7  Rdr 52(7)                                                                          WUPA
  1004936.0   1005110.6  Tag 08  00                                                                         
  1005656.6   1006008.3  Rdr 50  00  57  cd                                                             ok  HALT
  1069372.3   1069445.4  Rdr 52(7)                                                                          WUPA
  1515000.6   1515073.7  Rdr 52(7)                                                                          WUPA
  1515886.7   1516238.3  Rdr 50  00  57  cd                                                             ok  HALT
  1579601.2   1579674.3  Rdr 52(7)                                                                          WUPA
  2017453.7   2017526.8  Rdr 52(7)                                                                          WUPA
  2017619.2   2017793.8  Tag 08  00                                                                         
  2018341.0   2018692.6  Rdr 50  00  57  cd                                                             ok  HALT
  2082054.3   2082127.4  Rdr 52(7)                                                                          WUPA
  2519814.7   2519887.9  Rdr 52(7)                                                                          WUPA
  2520700.9   2521052.5  Rdr 50  00  57  cd                                                             ok  HALT
  2584417.7   2584490.9  Rdr 52(7)                                                                          WUPA
  3030027.1   3030100.3  Rdr 52(7)                                                                          WUPA
  3030913.3   3031264.9  Rdr 50  00  57  cd                                                             ok  HALT
  3094632.4   3094705.6  Rdr 52(7)                                                                          WUPA
  3532444.8   3532518.0  Rdr 52(7)                                                                          WUPA
  3532610.3   3532785.0  Tag 08  00                                                                         
  3533331.0   3533682.6  Rdr 50  00  57  cd                                                             ok  HALT
  3597056.0   3597129.2  Rdr 52(7)                                                                          WUPA
  4034805.9   4034879.1  Rdr 52(7)                                                                          WUPA
  4035692.0   4036043.7  Rdr 50  00  57  cd                                                             ok  HALT
  4099411.2   4099484.4  Rdr 52(7)                                                                          WUPA
  4545023.0   4545096.2  Rdr 52(7)                                                                          WUPA
  4545188.5   4545363.1  Tag 08  00                                                                         
  4545909.1   4546260.8  Rdr 50  00  57  cd                                                             ok  HALT


In the dump above I've noticed the same repeat pattern - phone issue WUPA command. Module accepts it and answer 08 00. Than phone decide to start whole sequence from the beggining and issue HALTA command (50  00  57 cd) and then WUPA(52) again.
First WUPA remains unanswered and phone issue WUPA command, that the PN532 answer this time. Phone restarts whole sequence after the answer.

And for first case we've got:

StartEndSrcData (! denotes parity error)CRCAnnotation
13121188.2  13121539.8  Rdr 50  00  57  cd                                                             ok  HALT
 13184913.3  13184986.4  Rdr 52(7)                                                                          WUPA
 13630572.3  13630645.4  Rdr 52(7)                                                                          WUPA
 13630737.5  13630912.1  Tag 08  00                                                                         
 13631458.4  13631810.0  Rdr 50  00  57  cd                                                             ok  HALT
 13695188.2  13695261.4  Rdr 52(7)                                                                          WUPA
 14132999.4  14133072.6  Rdr 52(7)                                                                          WUPA
 14133163.4  14133338.1  Tag 08  00                                                                         
 14133885.5  14134237.2  Rdr 50  00  57  cd                                                             ok  HALT
 14197602.4  14197675.5  Rdr 52(7)                                                                          WUPA
 14197767.6  14197942.2  Tag 08  00                                                                         
 14198488.5  14198670.2  Rdr 93  20                                                                         ANTICOLL
 14198757.5  14199191.7  Tag 08  00  00  00  08                                                             
 14199733.3  14200505.0  Rdr 93  70  08  00  00  00  08  f4  0f                                         ok  SELECT_UID
 14200597.1  14200861.4  Tag 60  f8  32                                                                 ok  
 14210462.5  14210814.2  Rdr e0  80  31  73                                                             ok  RATS
 14212232.4  14212831.9  Tag 05  75  33  92  03  ac  63                                                 ok  
 14223313.3  14223575.2  Rdr c2  e0  b4                                                                 ok  
 14225215.3  14225474.9  Tag c2  e0  b4                                                                 ok  
 14229224.8  14229297.9  Rdr 52(7)                                                                          WUPA
 14229390.0  14229564.6  Tag 08  00                                                                         
 14230110.9  14230882.6  Rdr 93  70  08  00  00  00  08  f4  0f                                         ok  SELECT_UID
 14230974.6  14231238.9  Tag 60  f8  32                                                                 ok  
 14231780.5  14232132.2  Rdr e0  80  31  73                                                             ok  RATS
 14233238.9  14233838.3  Tag 05  75  33  92  03  ac  63                                                 ok  
 14241905.6  14243272.0  Rdr 02  00  a4  04  00  07  d2  76  00  00  85  01  01  00  35  c0             ok  
 14250518.0  14250867.3  Tag f2  07  a7  25                                                             ok  
 14251410.0  14251761.7  Rdr f2  07  a7  25                                                             ok  
 14278827.1  14279256.6  Tag 02  90  00  f1  09                                                             


Looks like in successful case WUPA answer comes immediately after the first WUPA command, while in failed case only the second WUPA command gots answered. 

And there is a question - does anybody faced already wtih the same problem and how to solve it if it possible?

Thanks in advance.

0 Kudos
Reply
0 Replies