PN532 LOADMOD implementation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN532 LOADMOD implementation

1,939 Views
ivandodig
Contributor I

Dear NXP,

on our custom PN532 board we noticed that LOADMOD network is detuning the antenna when 1k resistors are placed.

When we remove them, the range doubles. 

We suspect that this is due to our NFET selection.

BSS138 have 13pF of output capacitance and this in series with 1kR introduces losses to the antenna? 

Would lower capacitance FETs solve this issue? Can you recommend us a SOT-23 capacitors specifically for LOADMOD circuit?

Also, can you confirm that LOADMOD circuit is needed for card emulation? We saw on few places that the IC can do card emulation without it, is this true?

The best solution for us is to remove the LOADMOD circuit altogether if it's not needed.

Thank you for your help.

Ivan

2 Replies

1,777 Views
carl1
Contributor I

We're having the same issue, would love to have an answer on this question.

0 Kudos
Reply

1,777 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Ivan, Carl:

The LOADMOD active circuit is optional in card emulation mode. The load modulation signals can be generated by the transmitter via the TX1 and TX2. See the application diagram from the datasheet:

pastedImage_1.png

Best Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply