PN532 CORE_INIT_RSP Field Value Questions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN532 CORE_INIT_RSP Field Value Questions

2,659件の閲覧回数
zeelivermorium
Contributor I

Hi,

I just started using PN7150 and want to understand some values in the CORE_INIT_RSP. The data is : 

CORE INIT RSP: 40 01 19 00 03 1e 03 00 08 00 01 02 03 80 81 82 83 02 d0 02 ff 02 00 04 88 10 01 a0

I have underlined the 4 bytes I am confused with. 

Byte 6: 1e, according to NCI 1.0, this is part of the NFCC features. 

pastedImage_7.png

All the NFCC bytes have upper 4 bits as 0. Why is there a 1 here? Shouldn't it be 0x0e?

Then the 0x81 0x82 0x83, I know 0x80-0xFE are for proprietary use, but in the user manual, only 0x80 is defnied 

pastedImage_9.png

What are the 0x81 0x82 and 0x83? And if they are some secrets, why bother putting it here anyway?

Thanks for your time and help in advance.

Best,

Z

0 件の賞賛
返信
4 返答(返信)

2,560件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please refer to the version 1.1 of NCI specification (1.0 indeed doesn’t define this bit).

 

In NCI 1.1:

pastedImage_1.png

Regarding proprietary bytes, they are not relevant in the response since not currently defined.

BR,

Ivan.

0 件の賞賛
返信

2,560件の閲覧回数
zeelivermorium
Contributor I

Hi Ivan,

Thanks for your response. However, I am conufsed since PN7150 should be an NCI 1.0 controller instead of NCI 1.1 right?

Best,

Zee

0 件の賞賛
返信

2,560件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

It depends on the firmware.

BR,

Ivan.

0 件の賞賛
返信

2,560件の閲覧回数
zeelivermorium
Contributor I

Typo in the title, PN7150 instead of PN532

0 件の賞賛
返信