PN5190 get invalid HF attenuator value on custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN5190 get invalid HF attenuator value on custom board

941 Views
Fanfei
Contributor II

Hi expert,

I am working on ulpcd mode on my board with PN5190.

It seems to need HF attenuator value by reading RX_CTRL_STATUS (0028h) register, but it always return 0x100401FC.

Are there any specific steps to do before reading?

0 Kudos
Reply
3 Replies

848 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Fanfei 

The following explanation should help you understand why the HF ATT value does not change:
RxP and RxN need to be connected to the antenna circuitry via a serial capacitor (for the DC decoupling) and a serial resistor (for the voltage level reduction). In combination with that external resistor, the HF attenuator block controls the RX input voltage level in such way that the RX always gets a proper input signal. This control loop is done automatically, and there is no direct user setting required.
Reading the HF_ATT_VAL (RXCTRL_STATUS register) retrieves a 6-bit value, which corresponds to the RX carrier input level, and therefore can be used to optimize some settings and adjustments.

0 Kudos
Reply

907 Views
Fanfei
Contributor II

Hi @KaiLi .

Thank you for reply.

My board can't connect NFC Cockpit.

0 Kudos
Reply

922 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Fanfei 

Can your board connect NFC Cockpit? If yes, please try :

KellyLi_0-1732003324203.png

 

0 Kudos
Reply