PN5190 Selecting Rrx.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN5190 Selecting Rrx.

1,482 Views
nike9307
Contributor II

Hi,
According to the "PN5190 antenna design guide" document, on point "6.1 Correct RX coupling" the way to tune the value of Rrx is to "4. Read H_ATT_VALUE, RX_CONTROL_STATUS register (0x28), bit 3…8" and change the resistor until its 40. 
In the current datasheed Rev. 3.5 that register doesn't exist, the closest i could find was the RX_CTRL_STATUS and RXCTRL_HF_ATT_VAL. Is it the same register described in the antenna design guide? 
EDIT: The HF_ATT_VAL and RXCTRL_STATUS names were also sued in the "PN5190 design-in recommendations" document. 

Also I believe there is a typo in the design guide, H_ATT_VALUE may refer to HF_ATT_VALUE, or vice versa. I'm not sure.  

On my test board, I'm getting 38 (dec) in that register. Should I aim for 40 exactly, or is 38 good enough? 

0 Kudos
Reply
1 Reply

1,444 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Nike:

 

Yes, you are right. there is a typo.  H_ATT_VALUE should be HF_ATT_VALUE.

RX_CONTROL_STATUS register (0x28)  ,  is RX_CTRL_STATUS.  Sorry a bit confusing. Thanks for your feedback. I will report it to the doc team.

danielchen_0-1669648753936.pngdanielchen_0-1669648753936.png

 

This value shall be ≈ 40 dec, so 38 is also ok.

 

Regards

Daniel

 

 

0 Kudos
Reply