PN5190 DPC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN5190 DPC

1,882件の閲覧回数
PDS
Contributor I

Hi. 

I saw "PN5190 Dynamic Power Control Quick Calibration and TxShaping Demo", but If I don't have to use PN5190 for payaments, and I have to use it with small labels ISO15693 or different size of Mifare tags, I think that DPC is not the best solution, or what is the best way to setup the PN5190?

Paolo

0 件の賞賛
返信
3 返答(返信)

1,856件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi PDS:

 

The Dynamic Power Control (DPC) is a feature that allows to control the transmitter current. Therefore the field strength depending on loading and detuning conditions. The DPC can be enabled and then dynamically adapts the output power.

DPC is a nice feature,  it offers an improved RF performance.  but it is not directly related to EMVCo.

 

Regards

Daniel

 

 

Regards

Daniel

0 件の賞賛
返信

1,853件の閲覧回数
PDS
Contributor I

Thank's Daniel for the answer. 

The advantages of DPC are clear, but is not simple to configure. Which is the best procedure for setup the DPC if I don't have to "use EMVCO settings".

Paolo

0 件の賞賛
返信

1,837件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi:

 

You can refer to AN 12549,  chapter 5:   PN5190 and DPC

PN5190 antenna design guide (nxp.com.cn)

 

 

Regards

Daniel

0 件の賞賛
返信