PN5180 with Renesas microcontroller. Communication SPI issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PN5180 with Renesas microcontroller. Communication SPI issue

2,781 次查看
sylvainung
Contributor I

Hello ,

I would like to have some help about using the PN5180 chip with a Renesas RX231 family (R5F52318ADFP)

I use 2 demoboard:

- PN5180 : PNEV5180B 2.2

- Renesas : YR0K505231S000BE

On the PN5180 board, I removed all connections between the LPC1769 and the PN5180 for the SPI(MOSI, MISO, SCK, SSEL, BUSY, PN_RST and PN_IRQ).

I have integrated the NxpNFCRdLib to my program on the Renesas Chip but it doesn't work.

This is my SPI configuration: 2Mbps, CPOL=0, CPHA=0.

The SPI configuration is correct because when I strap MOSI to MISO, I can read the value that I sent.

So I tried to read a register of the PN5180 without using the library.

I write on the register 0x00(32 bits) the value 0x0000AA55 for test.

On the oscilloscope I can see the MOSI frame.

But when I read this register (in debug mode) I received only 3 bytes instead of 4 and the 3 bytes are all 0x00.

Could someone help me please?

Thanks in advance.

0 项奖励
回复
2 回复数

2,447 次查看
nandyala_narend
Contributor I

And i want to know , the secure firmware upload and NFC cockpit  virtual COM port with other controllers...??

0 项奖励
回复

2,447 次查看
nandyala_narend
Contributor I

I think check with IRQ pin that ready signal to PN5180 from IDLE mode.

May be if you give before SPI command sent, enabling  the IRQ may gives you reply

Narender

9492828887 

0 项奖励
回复