PN5180 power consumption problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN5180 power consumption problem

2,961 Views
lu_xzh
Contributor I

Hello everyone:

I have a problem about PN5180.I hope you can help me,thank you

My question is below:

When the current consumption is 160mA, I use an oscilloscope to observe the antenna terminal voltage is only 32.48V,

Why is the power consumption so high and the antenna terminal voltage so low

Another question,Put the card on the coil and the power consumption reaches 244mA

The power consumption Shouldn't be lower when the card is on the coil?

Best Wishes

pastedImage_7.png

pastedImage_2.png

pastedImage_5.png

pastedImage_3.png

0 Kudos
Reply
2 Replies

2,875 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

In order to better service for you would you please  introduce the steps of testing you did, then I may replicate the phenomenon on my site.

0 Kudos
Reply

2,875 Views
lu_xzh
Contributor I

你好:

1、使用下面的板子,测试位置为发射端(图中红圈),使用示波器观察这儿的波形大小,测试峰峰值是40V,测试ITVDD功耗是160mA
Use the board below, the test position is the transmitting end (red circle in the figure), use the oscilloscope to observe the waveform size here, the test peak-peak value is 40V, and the test ITVDD power consumption is 160mA
我们之前测试别的芯片,测试发射端波形大小基本会有80V以上(TVDD功耗没有我们现在的大),这个波形峰值小的原因是因为DPC的因素吗?还是说本来就这么大,发射场强与这个发射端的峰值有直接的关系吗
We have tested other chips before, and the waveform size of the test transmitter will basically be over 80V (TVDD power consumption is not as large as our current power). Is the reason for the small peak value of this waveform due to DPC? Or is there a direct relationship between the intensity of the field and the peak at this end
2、DPC的功能也不是很清楚,所谓的动态功率控制,是不是我放卡在不同的位置,都会保持场强在一个合适的值,不是说过来或者过小。DPC验证的话,通过TVDD或者发射端峰值波形可以看出来什么变化吗
The function of DPC is not very clear, the so-called dynamic power control, whether I put the card in different positions, will keep the field strength in a suitable value, not to say come over or too small. If DPC is verified, what changes can be seen through TVDD or peak waveform at the transmitting end
谢谢
thank you

Catch(10-17-13-48-40).jpg

Catch0909(10-17-13-48-40).jpgCatch5711(10-17-13-48-40).jpg

0 Kudos
Reply