PN5180 interrupt handling in Library SW

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN5180 interrupt handling in Library SW

1,712 Views
smiwa
Contributor III

Hi,

Could you let me know how the library software detect and handle with IRQ from PN5180?

I like to know where jump table and its handler are written in source code in Llibrary:NFCReaderLibraryForCLEV663B-04.030.00.011627.

Thank you for your supports!

Best regards,

   S. Miwa

0 Kudos
Reply
3 Replies

1,501 Views
smiwa
Contributor III

Hi Kan san,

Very sorry... It is typo. The device is PN5180 and its library is also for PN5180. Not for CLEV663.

Thank you very much!

best regards,

   S. Miwa

0 Kudos
Reply

1,501 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi S.Miwa,

Thanks for the information! Please kindly refer to the following for details.

pastedImage_1.png


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,501 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi S.Miwa,

Would you please clarify which chip you are referring to? PN5180 or CLEV663? Thanks for your patience!

B.R

Kan

0 Kudos
Reply