PN5180 Should I increase or decrease the coupling resistors to increase AGC_VALUE?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PN5180 Should I increase or decrease the coupling resistors to increase AGC_VALUE?

跳至解决方案
3,444 次查看
oferrer
Contributor I

Hi,

I am immersed in the process of optimizing the receiver but I´m a little confused about it.

AN11740 - 4.5.1 External RX components says to increase R1A and R1B if AGC_VALUE is low (<250)

but AN11742 says:

-1.2.4.1 Step 1: Unloaded. The Rx resistor was chosen to be R = 3.0 kΩ. The measurement shows the AGC value of 369 in gear 0, driving ITVDD = 139mA (unloaded). The recommended AGC value is 300, so in this case the Rx resistor could be slightly increased.

-7 Annex, Table 13 "The Rx resistor = 5.1kΩ, so the nominal AGC value unloaded is too low."

-7 Annex  ...However, here the AGC values are lower, since a higher Rx coupling resistor has been used."

 

So, should I increase or decrease the coupling resistors if AGC_VALUE is low (=139)?

Currently, the chosen resistor are 4.7kOhm, as recomended as starting point.

Thanks,

0 项奖励
回复
1 解答
3,367 次查看
Fabian_R
NXP TechSupport
NXP TechSupport

Hello sir,
My recommendation when using DPC is to please follow AN11742 steps, you can start with a 3kΩ and adjust, If the AGC value is too high, increase the Rx resistor value.

Best Regards,
Fabian

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,336 次查看
oferrer
Contributor I

Thanks @Fabian_R for your answer,

I had to use an even lower value (2,2kΩ) to get the minimum AGC_VALUE required.

Maybe this low value has to do with the selected high target impedance (battery powered handheld device).

So, i had to decrease coupling resistor in order to increase AGC_VALUE. DPC calibration is now done.

Thanks again.

Osmany

0 项奖励
回复
3,399 次查看
Fabian_R
NXP TechSupport
NXP TechSupport

Hello sir,

Please keep in mind that these are recommendations that may vary on your design and requirements.  These component values should be selected according to the antenna characteristics and your measurements.

Please take a look at our NFC Antenna Tool for a quick recommendation of the components of your antenna.

I also want to recommend to please take a look at our Antenna design video series which shows the iterative process for successfully designing your matching circuit along with the proper calibration and, fine-tuning using NFC Cockpit.

Best Regards,
Fabian
0 项奖励
回复
3,395 次查看
oferrer
Contributor I

Thanks @Fabian_R  for your answer.

My circuit board (prototype) is already printed with pn5180 and a customized antenna on it. NFC Antenna Tool was used for maths (no RX resistor calculated). Now, it's running well. 

As i said, i'm optimizing receiver before production. I need to change RX external resistors (1kohm-10kohm) to get optimal AGC_VALUE 600 (ANT1/ANT2 were not connected, pure read mode).

I need to increase AGC_VALUE. That's why my question. 

Should I increase or decrease external coupling resistors in order to increase AGC_VALUE?

Is there any contradiction between AN11740 4.5.1 AND (AN11742 Table 5 Example OR AN11742  Table 13 Example)?

Thanks in advance,

Osmany

 

 

0 项奖励
回复
3,368 次查看
Fabian_R
NXP TechSupport
NXP TechSupport

Hello sir,
My recommendation when using DPC is to please follow AN11742 steps, you can start with a 3kΩ and adjust, If the AGC value is too high, increase the Rx resistor value.

Best Regards,
Fabian
0 项奖励
回复