PN512 with MIFARE Plus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN512 with MIFARE Plus

18,214件の閲覧回数
mindaugasspelve
Contributor I

Hello,

I am developing functionality, that handles communication between PN512 reader and MIFARE Plus tag. I encountered two problems:

1. NXP lacks of documentation on MIFARE Plus tag. And signing NDA to get more information about tag is slowing development down (are there any other options?);

2. PN512 reader library does not include  phalMfp component (MIFARE Plus tag layer). If you google a function name phalMfp_Sw_Init you would find two GitHub repositories that hold NFC reader library with phalMfp component. My question is, where could I get the official version of phalMfp component.

Thank you.

タグ(3)
0 件の賞賛
返信
4 返答(返信)

17,535件の閲覧回数
mindaugasspelve
Contributor I

Hello,

I have signed NDA and got access to docstore. I found library for NXP reader PN512 with phalMfp component for MIFARE Plus. But I can't find any example on how to use this component, how to initialize it, how initialize other components, that phalMfp component depends on. Can you please guide me on what documentation should I use or maybe there is an example source code.  

Best regards.

0 件の賞賛
返信

17,535件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Mindaugas,

I am sorry, but if you got access to docstore, haven't you found the following docs and sample codes?

pastedImage_1.png

if not, maybe your account didn't have permission to these materials, please contact the support for docstore to help with it.


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

17,313件の閲覧回数
Viktor_
Contributor I

can't find any example on how to use this component, how to initialize it, how initialize other components, that phalMfp component depends on

Have the same question.

And can't find this documents on DocStore -> MIFARE ICs -> MIFARE PLus EV2 folder

 

I have Full access with "High" rights.

 

I have only:

Ds522332

Ad580931

An576410

An576310

An576211

An576010

An575910

 

And don't have:

Um175821

Um172903

Sw166910

etc.

 

Where can I find them?

タグ(1)
0 件の賞賛
返信

17,532件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Mindaugas,

NDA is the only channel to fetch the related documentation and full reader library including phalMfp component, after sign the NDA, you may register a docstore account, and apply for the doc as well as the full library. You may contact your local DFAE for NDA assistance. Please refer to Distributor Network|NXP and the attachment for details.


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信