PN512 ReadRegister and WriteRegister commands

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN512 ReadRegister and WriteRegister commands

1,295 Views
avgurt9
Contributor I

Hello,

The PN532 microcontroller has the ReadRegister (D4 06 ADRh ADRl) and WriteRegister (D4 08 ADRh ADRl VAL) commands.

For smart card reader ACS ACR122U, they can be used, for example, as

FF 00 00 00 04 D4 06 63 05

and

FF 00 00 00 04 D4 08 63 05 04

 

Are there similar commands for the PN512 microcontroller (smart card reader ACS ACR1252U)?

 

 

0 Kudos
Reply
1 Reply

1,264 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

 

All the information available from commands to software examples can be found in the web page of the device PN512 | standard NFC frontend | NXP Semiconductors or the NFC Integrated Solution | NXP Semiconductors in case you are using this other one. 

For the other reader set of commands, please reach out to the manufacturer. 

 

Regards,

0 Kudos
Reply