P2P mode through 14443

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P2P mode through 14443

2,743件の閲覧回数
bhargaviunnamat
Contributor I

Hi Team,

Please clarify if NT3H1101 will support sharing GPS data through NFC. We would like to share the Mobile Phone location through NFC. As NT3H1101 supports 14443 read/write mode, shall i able to read data from mobile phone of GPS data? Or do i need to use PEER to PEER mode tag? If yes, Kindly suggest P2P supported I2C TAGS for my application.

タグ(3)
0 件の賞賛
返信
3 返答(返信)

2,568件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

I believe there is a terminology confusion between the P2P, tag, reader, etc.  

Could you please watch the following webinars which will help to clarify the concepts?

NFC Essentials Webinar|NXP 

NFC Applications and Use Cases|NXP 

I believe you will find also there which will be the best product to use, nonetheless, if you have any further question, let me know. 

Regards, 

Estephania 

0 件の賞賛
返信

2,568件の閲覧回数
bhargaviunnamat
Contributor I

Thanks Martinez. We have gone through the two webiner session. We have selected NTAG I2C TAG - NT3H1101 , which is best suite for our present application. Which is connected to Controller and NFC antenna, such that it will able to communicate to/from Phone APP.

0 件の賞賛
返信

2,568件の閲覧回数
bhargaviunnamat
Contributor I

Please help this out.

0 件の賞賛
返信