Originality Signature Generation ALgorythm

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Originality Signature Generation ALgorythm

982件の閲覧回数
KimStanley
Contributor I

Hi,

I'm investigating the Originality Signature of SLIX2.

Which data should be encrypted with NXP's private key to obtain the originality signature?

How is signature verification performed?

0 件の賞賛
返信
1 返信

961件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @KimStanley 

For Signature Verification, which needs the following inputs:
1) Public Key, that is saved in the dedicated file. As long as you sign an NDA with NXP, you can get it.
2) Signature and UID, two are unique to NXP products. They are stored in a hidden area of the chip and can only be read through dedicated commands.
3) Algorithm, ICODE used is ECDSA, which is an open-source algorithm. The source code can be downloaded on GitHub.
Hope them helps.
BR
kelly
0 件の賞賛
返信