OM5578 on Raspberry Pi 3 Model B

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OM5578 on Raspberry Pi 3 Model B

2,146 次查看
luca_mazzara
Contributor I

Hi

I bought the board OM5578 and a Raspberry Pi 3 Model B, I downloaded "OM5578-PN7150S_Rpi_Linux_demo_v1.2" image. But the raspberry didn't boot, the monitor shown a thunder and a red led on the rasperry blinked (power not enough) I'm using a power supply 5Vdc 2.5A. If I install the RASPBIAN image, the raspberry boots normally with same hardware setup (power supply, monitor etc). what is going wrong?

0 项奖励
回复
1 回复

1,945 次查看
jimmychan
NXP TechSupport
NXP TechSupport

This image can work on Rasp. Pi 2.

I think the issue is due to the I2C pins setting on Pi 3.

You can try to build the new image for this board.

You can refer to this document.

https://www.nxp.com/docs/en/application-note/AN11697.pdf 

0 项奖励
回复