OM5578 on Raspberry Pi 3 Model B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OM5578 on Raspberry Pi 3 Model B

2,142 Views
luca_mazzara
Contributor I

Hi

I bought the board OM5578 and a Raspberry Pi 3 Model B, I downloaded "OM5578-PN7150S_Rpi_Linux_demo_v1.2" image. But the raspberry didn't boot, the monitor shown a thunder and a red led on the rasperry blinked (power not enough) I'm using a power supply 5Vdc 2.5A. If I install the RASPBIAN image, the raspberry boots normally with same hardware setup (power supply, monitor etc). what is going wrong?

0 Kudos
Reply
1 Reply

1,941 Views
jimmychan
NXP TechSupport
NXP TechSupport

This image can work on Rasp. Pi 2.

I think the issue is due to the I2C pins setting on Pi 3.

You can try to build the new image for this board.

You can refer to this document.

https://www.nxp.com/docs/en/application-note/AN11697.pdf 

0 Kudos
Reply