OM25180FDK and NFC cockpit getting started

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OM25180FDK and NFC cockpit getting started

1,485 Views
koenvandeven
Contributor I

Hi,

How can the card supplied with the OM25180FDK be read?

What is the sequence of commands using NFC cockpit v3.7.0 FW: v3.6.0, EE 147.0.0?

I can't seem to find a getting started guide except AN11744.

I believe the supplied card that comes with the  OM25180FDK  is a type F card.

So my sequence (from the NFC cockpit log Monitor):

[2017.05.11 12:30:44]:INFO:TypeFCardViewModel:RM_F_212 Protocol loaded successfully.
[2017.05.11 12:30:47]:INFO:RfFieldControlService:RF On
[2017.05.11 12:30:49]:ERROR:RFProtocolTypeFService:GetIDmPMm : HAL,INTERNAL_ERROR

If this works I would like to read the NTAG 213 that will be integrated in a product of ours.

Any idea how I could accomplish this using the  OM25180FDK  and NFC cockpit v3.7.0 without having to write software?

Thanks

0 Kudos
Reply
1 Reply

1,204 Views
IvanRuiz
NXP Employee
NXP Employee

Dear Koen,

Please refer to the following link: https://community.nxp.com/thread/437484 

Best regards,

Ivan.

0 Kudos
Reply