Nfc reading speed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Nfc reading speed

1,533 次查看
schakoma
Contributor I

Hello all. I am using the CLEV6630B evaluation board as a reader. The board has CLRC663 nfc chip. I'm trying to read ECG data from the NTAG12C. I'm using example 9 of the nfc reader library. The reading speed is a bit slow. Are there ways of increasing the reading speed? What is the maximum SRAM communication speed of the clrc663 chip?

Thank you 

0 项奖励
回复
1 回复

1,502 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello @schakoma .

You can refer to the example of SW6693 as the link if you just  read ECG data from the NTAG.

There is not the NFC library of SW6793. So doesn't the time to porting the library.

Have a nice day.

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 项奖励
回复